Hi. we've successfully developed 5kW Interleaved PFC with UCC28070 and planning to parallelize it to make 10kW.
And If I understand the answer from this link correctly, there's no function to parallelize 2 ucc28070 without "Synchronized Clocks with 180° Phase Shift"
If there's no option to use internal clocks or function to parallelize 2 UCC28070 without external circuit, Do you have any suggestions for "Synchronized Clocks with 180° Phase Shift"?
Best regards.