Dear reader.
I made my own PCB with the following schematic:
C10(value C10) and C8(value C9) are not solderd
With my first and only solderd PCB i did a test.
Test TPS65130 1st PCB solderd
Cheap multimeter borrowed from school (Peaktech 3340 DMM)
Vin = 3.3V @ 129 mA
Vout positive = 8.10V
Vout negative = -12.16V
ENP = PSP = ENN = PSN = 3.3V
FBP = 0.826 V
FBN = -0.120 V
Vref = 1,227 V
Before positive diode = 3.27 V
The problem is that i made this circuit to convert 3.3V to +12V and -12V.
I only get +8V and -12V. My problem is why do i get the +8V and what do i need to change to get +12V?