Hello Team,
I would like to understand that the delay time during OVP condition when CD cap is opened. Is that same of tCD_GND?
Regards,
Kotaro Yamashita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
I would like to understand that the delay time during OVP condition when CD cap is opened. Is that same of tCD_GND?
Regards,
Kotaro Yamashita
Hi Kotaro,
When the CD capacitor is opened, the pin and trace will still have some small capacitance. See equation 1 in the data sheet for calculation in http://www.ti.com/document-viewer/BQ2947/datasheet/external-delay-capacitor-cd-slusb153980#SLUSB153980
If the residual capacitance were 100 pF, the delay expected would be 1 to 2 ms. Note that this is faster than the customer test mode which is a recognized by the shorted condition. Internal delays may limit the time of very small capacitances.