Hello,
I want to detect charging current of BQ25150.
my battery configuration are as follow :
1) battery voltage setup = 3.7 V
2) charging current Pre : 42.5 mA
Fast : 350 mA
I had use reg 0x46 & 0x47. to detect this.
The ADCDATA_ICHG = 13301.
& according to formule => (13301 / (0.8*65536))*100 = 25.37 %
But my charging current is 350 mA.
Is there another way/formula to find what is charging current ??
/ Akshay P