This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 88
Part Number: ATL431
HI,Is the ATL431 made on a CMOS or bipolar process?The reason for asking is I want to use it for a high radiation environment.Thanks!
Hi Jason
ATL431 uses bipolar process. I will confirm experts and let you know if it is safe for radiation.
Regards
Trailokya
In reply to Trailokya Rai:
HI Jason
ATL431 is safe for radiation environment.
Thanks!!May I ask if you have more detail re: "safe for radiation"?Is this an educated guess? Do you have guesses for TID or SEE performance? Actual data?Thanks again!
In reply to Jason Cuadra35:
Hi Jason,
Our devices that have TID or SEE or any rad certification have it on the datasheet. I believe we initially misunderstood the question about radiation since some applications do not need certification. We do not have RAD data for TL431 that was listed above.
The only TL431 like device that is radiation certified is the productions below.
TL1431-DIE or TL1431-SP. See datasheets below for the products that can support certified radiation certification as listed on the datasheet..
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
If you feel your thread is resolved, please selected Answered.
Looking for the lowest noise voltage reference? Check out the new REF70 family of products starting with the REF7025 with 0.22 ppm p-p of noise.
Check out: Voltage Reference Design Tips For Data Converters a new app note that discusses voltage reference error and how it affects ADCs/DACs