Other Parts Discussed in Thread: TPS61022, TPS62740
Hi,
I shall design a Power Back Up (PBU) function for 60s at 4W (5.1V 800mA) with super capacitors (charge time 180s)
General: Vin 12V to 34V.
I'm considering to use LMR33610 in two different ways. One to bridge the charge time second to charge the Super-cap:
1) Generate 5.1V 0.8A. (Generate 5.1V during the charge time for the super-cap).
After about 160s the TPS61022 starts and generate 5.2V in parallel with the above voltage.
Will this cause the LOW fet side in the LMR33610 to turn ON shorting the output or will the IC go into PFM mode both fets Off???
During the PBU time the voltage regulator has 5.2V at the output and 0V at the input.
In order not to backdrive voltage from the output back to the input rail I consider to place a diode in serial with the input voltage (pin 2) is this required?
Will there be drawn current back into the LMR33610 in this case?
2) Charging the super-caps.
I need to charge the super-cap from 0V to 4.6V with 0.8A.
Can you propose a simple (Low: comp. counts and low PCB arear and moderate cost) circuit that give the FB pin 5 a pre-bias regulating the output current to about 800mA +/- 5%?
FYI the above is related to #refid:d6cb966c-fedc-447d-adbb-413bd6a7936f
Br
Jørgen