We are using this IC to generate 1.5V & 1.8V individually from 3.3.V.
Need the rise time & fall time of the internal FETs to calculate the switching loss.
Also, if there is short at the output side, will the IC retry after certain time. Or will the IC latch off? Based on datasheet, As soon as the switch current-limits are met and the output voltage falls below 1/3 of the nominal output voltage because of overload or short circuit condition, the foldback current-limit is enabled. In this case the switch current-limit is reduced to 1/3 of the nominal value ILIMF. Will this operational cycle repeat? Or, will it stop after the first iteration?
Thank You,
Vignesh T