Hi,
I need to design a power supply divided into 4-5 modules connected in parallel, each module needs to produce an output power of about 400W.
Vin = 24V (but if there was a solution covering the range also 12V could be interesting)
Vout = 150V
Need for the output to be isolated from the input (may be thru a transformer?)
Automotive components are preferred even if the application is industrial.
Preferable use of integrated ICs... we would prefer to avoid a solution that needs DSP / microcontroller
Any comments?
Many Thanks,
Antonio