Other Parts Discussed in Thread: TPS62088, TPS62095, TPS62810-Q1
Dear Sir,
Please advise if there has one part has better efficiency than TPS62135 at the condition of 5.6Vin, 3.8Vout, 3~4A Iout.
Feature needed :
100% Duty Cycle mode
Power Good Output
Vin is 4V~6V
Iout 3 ~ 4A
Suppose TPS62088 or TPS62095 may be better, but it's input only up to 5.5V. Target operate Vin need to be 6V or 6.5V.
Thanks,
Hugo