Hi team,
I saw the PMbus interface supports either 3.3V or 1.8V voltage level. Where to set it?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I saw the PMbus interface supports either 3.3V or 1.8V voltage level. Where to set it?
Thanks.
Hello, there is not a setting or pinstrap as such. The VIH and VIL levels are set up such that the logic is compatible with either pull-up voltage, and the pull-down on the data pin is strong enough to pull down to the logic low level. Note in the SMBus v2.0 spec high power DC specs, there is only one spec for pull-up voltage of 1.8V to 5V.