I'm using UCC21530 to drive a synchronous buck converter (500V to 200V). Considering the parasitic inductances and to keep the gate-source voltage below the threshold voltage level, I'm using Zener diode to provide negative bias. There is no specific guidance on choosing the current limiting resistor connected in series with the Zener. I'm using 51ohm resistor. For some reason, I'm facing convergence problem while simulating it under transient mode. It stops at 56%. Will you be able to guide me on this? I have attached screenshots of my circuit and the output.