Other Parts Discussed in Thread: TPS61088
Hi Helen,
Do you care about the capacitance of a capacitor? Or ESR?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Helen,
Hello user6265022,
There is not really a relationship to the inductor, but if you make the inductor smaller, the peak current increases, so the burden on the input capacitor increases as well. In general it is important that it is placed close to the IC to minimize input impedance.
The ESR has to be small to minimize voltage ripple, so we recommend10uF capacitance with ceramic capacitors. Be aware of the DC bias effect of ceramic capacitors.
Dear Sir,
Thanks Brigitte!
The selection of inductor related to the Vin, Vout, Io and the operation frequency. For the boost converter, the selection of inductor and capacitor have no direct relationship.
What is your Vin, Vo and Io? We can help to select the inductor for you.
Hi Helen,
Dear Sir,
For the TPS61088 or TPS61088-Q1, ESR is not a must. So only ceramic cap at output side is also OK.
If there's no dynamic requirements, you can choose 2 pcs 22uF/25V/1210 ceramic cap at the output side. if you need to choose smaller size cap, then you need to place more caps at the output side because of the derating under 12V DC bias.