Hi team,
Vin=5V, Vout=1.8V, Iout=0.5 to 1A Fsw=2.1MHz
If I calculate inductance based on 30% inductor ripple current, the inductance should be around 1.8uH.
So I would like to use 1.8uH to 2.2uH coil for LC filter with matched output capacitance.
But the datasheet suggestion is about 0.47uH to <1uH.
Is there any restrictions increasing the inductance?
regards,