Hi Team,
Customer is evaluating TPS23756 and customer has PCB size concern.
Would you please provide suggestions for this request?
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Customer is evaluating TPS23756 and customer has PCB size concern.
Would you please provide suggestions for this request?
BR,
SHH
Hello,
The PCB is an EVM, which has numerous test points and jumpers that can be removed. This also frees up space for other components to be moved in. Additionally, the customer could choose to use a PCB with more layers so that more components could be placed closer together. They could also simply try the same design but improving the layout. The power flow of the EVM is a clear, left to right flow. They could try a "C" shape or an "L" shape instead.
All of those suggestions are using the same, proven design with all the same components. Another path is to use a smaller transformer. I do not recommend this, as smaller transformers typically translates to worse performance. Since the transformer is so essential to the design, careful attention to surrounding components must be used to ensure proper operation. But this is a path to a smaller design.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments