Part Number: LMZ31710
Other Parts Discussed in Thread: UCD9090A, , TPSM84A21, LM10010, TPSM846C23
Hello,
I am using the LMZ31710 currently in a design and I am fixing the output voltage using the rset resistor. I also use the UCD9090A, to sequence this supply and to margin voltages on some linear supplies. I wanted to know if I could add a margining circuit from the UCD9090A to the VADJ pin so that I could move the output voltage up/down depending on the requirements. I am looking at a range of perhaps 1.1 to 1.9V output.
If so is there an example design that I could look at.
Or is there another supply that you could recommend that could be controlled directly via a PMBus?
Regards,
Guy