Other Parts Discussed in Thread: CSD95482RWJ,
Dear all,
I woud like to ask about CSD95480RWJ and CSD95482RWJ.
I'm requesting a detailed data sheet, but our customer wants an answer as soon as possible. Could you please tell us the following questions?
・ I want to know how to determine constants for peripheral components when using CSD95480RWJ and CSD95482RWJ.
For example, the resistance value and inductor value attached to LSET.
(The red circle in the figure below.)
・ Check that CSD95480RWJ is a product that can output up to 70A.
If you check the following figure, you can use it even if the output current is 10A or less. Is it possible that PWM control cannot be performed under these conditions?
Best Regards,
Y.Ottey