Hi,
I'm using a UCC21530 for a university project for a buck converter to convert 500V to 200V.
I'm trying to power a UCC21530 using a linear voltage regulator for VCC, VDDA and VDDB.
My design is for the converter is based on figure 39 of the datasheet:
The design is working fine without the linear regulator.
I'm trying to use a TPS7A4501 to regulate the Vdd and Vcc, but I cannot figure out how to use it since the zener is connected to the negative side to the voltage supply and the regulator only has one output pin.
I have tried several ways to connect it but none have worked. This is my current schematic:
NMOS_buck_zener - autosave 20-03-26 23_16 - autosave 20-03-28 13_55.TSC
What should be the correct was to insert a voltage regulator in this design?
Thanks,