This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 33
Part Number: TPS7A49
Hi
TPS7A4901DGNR: what's the Vout(nom) value in Vdo item?
thanks.
Hi Max,
VOUT(NOM) is the target regulation voltage. Meaning if VOUT was set to 5V, VDO is measured with VIN = 4.75V and with a load current of 150mA, VOUT could be as low as 4.15V (5x0.95-0.6=4.15).
I hope this helps to clarify.
John Cummings 蔣康明Texas Instruments 德洲儀器Johncummings@ti.com
Please click the "Resolved" link at the bottom of this post if I have answered your question.
Thank you,