Hello,
I am trying to find out the values for the resistors in the voltage dividers between V_SEN and PH pins (R1 and R2).
The above diagram is given in page 1 of the datasheet http://www.ti.com/lit/ds/symlink/tps54821.pdf.
As per the given equation 1, which is the resistor R5 and R6 in the above diagram.
Although the equation refers to figure 29, I don't see R5 and R6 labels placed correctly there.
For example, the example in Figure 29, it needs 3.3V output, and applying equation 1 to it, R5 = 10^4(3.3-0.6)/0.6 = 45kOhm, but the figure shows 2.2kOhm resistor.
Could someone please clarify this bit for me, perhaps by revising the equation with respect to the above equation.
My need is to output 12V for which I am needed to find the resistor values.
Thanks,
Naveen.