Hello
I Designed using TPS62802 under the following conditions
VIN : 3.1V ~ 3.2V
Vour : 3.0V
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I Designed using TPS62802 under the following conditions
VIN : 3.1V ~ 3.2V
Vour : 3.0V
Best Regards.
Hi,
There is an automatic transition to PFM mode when the converter has light load conditions if you enable Power Save mode.
You could only choose to enable the Power Save Mode mode or Forced PWM mode. The boundary between PWM and PFM mode is when the inductor current becomes discontinuous.
Regards,
Febin