Part Number: LM1085
Dear all
I woud like to ask about output capacitor of LM1085.
After reviewing the LM1085 data sheet, the data sheet recommends that the output capacitor be 10uF tantalum or 50uF aluminum electrolytic.
After confirming the following application notes, we are currently considering connecting an ESR resistor in series with a ceramic capacitor as the output capacitor.
Please answer the following questions:
http://www.ti.com/lit/an/slva214a/slva214a.pdf
1. Is it recommended that the recommended capacitance when using a ceramic capacitor is 10μF or more?
2. From the formula (1 / ESR × C) in the following post, the minimum ESR required was confirmed to be at least 0.2Ω when the capacitance is 10μF.
Is there no problem with the above method?
https://e2e.ti.com/support/power-management/f/196/t/862307?tisearch=e2e-sitesearch&keymatch=LM1085
If not, what is the minimum required ESR value?
(In addition, please tell me the ESR resistance required when using a low ESR ceramic capacitor.)
Best Regards,
Y.Ottey