This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sheldon,
Please make sure that the PCB is clean.
If there is a leakage path through an unclean board to the NR/SS pin, the NR/SS voltage can charge beyond the reference voltage.
This would have the effect that you are describing.
We see this occasionally from customers and it usually goes away once the board has been cleaned.
Thanks,
- Stephen
Hi Stephen:
Once 3.3V EN and 4.8V BIAS applied to TPS7A8300 after VIN 1.2V, no such failure happens to the part anymore and Vout = 1.0V as expected. Definitely the failure mode didn't have the part demaged.
But there is no explicit statement require this knid of timing sequency in the datasheet of TPS7A8300. Could you verify if there is some timing sequence requirement for TPS7A8300. Thank you,
Sheldon
Hi Sheldon,
We might need an oscilloscope plot here showing Vin, Vbias, Vout, and either SS or EN.
Is that something we can get?
In particular I would like to see the timing you are describing.
So the LDO fails to operate correctly then after the right conditions are applied, it regulates as expected.
If this requires multiple oscilloscope plots, that is also fine.
Thanks,
- Stephen