Part Number: TPS54620
Hello E2E,
My customer needs to ensure that EN is held low until a micro enables the TPS54620. However the micro is powered up after 12V is applied to TPS54620. They want to add in a pull down resistor to hold the EN line low, however, they are curious as to how they should size the resistor. Do you have any suggestions on the value to resistor to use? They are open to other methods to ensure that the TPS54620 is held low until the micro enables it.
Also, the micro is using a push/pull output and I can across this thread discussing the need for a protection resistor in series:
Thanks!
Russell