I am using LP2951, with fixed output voltage as 3.3 V. the input is 14.4V and i have connected the out and sense pin together. also thefdback and vtap pins are connected together to obtain a fixed output voltage. however i am measuring an output voltage between 1.05-1.15V, and it is not fixed and fluctuates within this range. I have attached a schematic diagram for reference. please tell me how can i obtain a fixed output voltage of 3.3v