Hello,
Sadly no charging of the battery (3S1P with 3Ah) is possible (ACOK is high).
Also the BATDRV Output is always 0V (Even if the AC Adapter is not present).
I am using as AC Adapter a lab PSU (24V Current Limit @ 2A)
When iam using your Evalboard everything is working fine.
The system load is only a tiny 3.3v StepDown Regulator for the MCU.
I have attached the schematic and a part of the layout.
With friendly regards
Mark RudolphBS2000-M4-PSU-039_SCH.PDF