Other Parts Discussed in Thread: BQ24040
Hello,
We have a problem with the BQ24210. We use the following schematic:
Whenever we connect a USB wall charger we measure Vbus = 5V, ~EN = ~PG = 0V (J8 is mounted) but the battery(1S2P or 1S3P), connected to K6, is not being charged.
Vbat = 0V, due to the battery being in protection mode. Protection mode will release when a charger is connected. This is tested; applying a positive voltage to the battery + terminal releases the protection.
VDPM, ~PG(and so ~EN_CHR) and ~CHG are connected to high impedance uC inputs.
Can someone please advise on this?
If needed, I can provide additional measurement data, please let me know.
Thanks in advance,
Sander Baten
Embedded System Engineer