Part Number: BQ24105-Q1
Hi TI-team
My customer has some question about OPERATIONAL FLOW CHART
Would you give me an answer ?
1, About the judgment criteria of "VBAT<VLOWV" when "FSTCHG Timer Expired ?" is No.
If it is VLOWV, i think the threshold voltage of the precharge judgment standard.
Isn't it a mistake of VOREG-VRCH ?
2, In this flow chart, it seems that it will not return to the recharging flow (the beginning of the flow) unless it detects that the battery has been removed from the state that charging is completed.
If the voltage drops due to discharge even if the battery is not removed, will it return to the recharge flow ?
Will it not be recharged without "POR" ?
3, About each “Suspend Charge” on the flowchart
Is the waiting time fixed ?
4, About "ITERM detection?"
If the charge termination current (ITERM) cannot be detected after charging and the result is "No",
does it mean that the loop of "Regulate Current or Voltage" -> "TS Pin in LTF to TCO Range ?" -> "FSTCHG Timer Expired ?" -> "VBAT<VLOWV" -> "ITERM detection ?" are continued until "POR" ?
Best Regards,
Koji Hayashi