This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27511: max. junction temperature

Part Number: UCC27511
Other Parts Discussed in Thread: UCC23511

Hi Team,

  My customer would like to know UCC27511 max junction temperature spec. Would you please help for it? Or can I assume and use 150°C for the Tj max.

 Note. From datasheet that one list the recommend Operating junction temperature range is –40°C to 140°C and Tstg is –65°C to 150°C.

Best regards,

Albert Lee.