Can the TPS2051B be potentially damaged when 5VDC is applied to its outputs and the device is not powered? I am curious for the transitions not only on the output, but also on the power of the TPS2051B itself. Could there be any specific case that could create a damaging operating condition for the device?
I understand that the TPS2051B may or may not prevent reverse current in case the outputs have 5VDC applied to them (it will depend on the enable pin). That is not a concern for this application however.
Thank you!