I am now reading the UCC28780 data sheet. I have a question about LC filter design. You are using ceramic capacitors 33uF / 25V in parallel.
It also states that the ESR should be very low.
However, the actual capacitance value is several uF. ‥
Since I design Vout at 32V, I need a ceramic capacitor of 35V or more. If the requirements are only a few uF and low ESR, how about using the MU series (35V, 4.7uF) of POLYMER MULTI-LAYER CAPACITORS (RUBICON) as an alternative to ceramic capacitors? (MU35 / 4.7 ≈ Ceracon 33uF × 2)
Of course, it is not as low ESR as Ceracon, but it is also stated in the manufacturer's HP that it is quite small.
We believe that alternatives will contribute to downsizing.
Ceramic capacitors also care about destruction due to mechanical (shock) cracks.
Please give us your opinion.
B.R. Tak