Hello ,
I want to read battery charging current in pre-charging mode.
In BQ25150's data sheet, the formule is as -> %ICHARGE = (ADCDATA_ICHG*100)/0.8*65536.
But this is for fast charging current.
Battery charge current in PRE = 22.5 mA & In FAST = 110 mA.
Pre-to fast threshold = 3 V.
If battery voltage is 2.8 then it gave 110mA.why ??
How to detect battery charge current in pre-charging mode ??
/Akshay P