This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570EVM-206 : BQ25570 Rin Q&A

Prodigy 190 points

Replies: 1

Views: 28

Part Number: BQ25570EVM-206

I have a question about the Rin on the bq25570 evmboard.

I think the value of Rin, the resistance to the VIN_DC terminal on the board, is 2.27k ohms.

I want to know exactly how much this is.

1 Reply

  • Guru 92160 points

    Hi Sanghyun,

    Are you referring to the resistance from VIN_DC pin to GND when VSTOR=0V?  We haven't characterized that value.

    Keep in mind, there is an NFET from VIN_DC to ground that turns on if VIN_DC=VMPP > VBAT_OV to prevent over-voltage on the storage element.

    Regards,

    Jeff

    Please click "This resolved my issue" button if this post answers your question.

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.