Other Parts Discussed in Thread: PMP15037
Dear all
I would like to ask questions about LED PWM dimming using TPS61087.
Our customer is trying to do LED dimming by inputting a 200Hz pulse signal to the EN pin as in the following application example (listed in the TPS61087 data sheet).
I would like to know about the following contents.
①By checking the above circuit example, I think that the above dimming is possible.
Is this possible even if the conditions such as input / output voltage change?
* By the way, our customers are trying to implement under the following conditions.
Vin = 3.0V-4.2V
Vout = 6.5V (or 6.0V)
Iout = 1.0A
Fsw = 650kHz
② Is there any concern when dimming the LED by inputting a pulse signal to the EN pin as in the above circuit example?
(I think it is necessary to pay attention to the responsiveness such as making the value of Rcomp larger than the calculated value of the data sheet.)
Best Regards,
Y.Ottey