This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: Current detection method

Part Number: UCC28070


Hi,

I am considering using UCC28070 device.
Regarding the current detection method of UCC28070, I would like to detect the current by inserting a low resistance on the source side of the FET as shown below, instead of the current transformer method of the recommended circuit.
Is such a method of current detection possible?
If so, is there a TI current sense amplifier that is the best choice for sensing?
I am going to use the VCC of UCC28070 (I plan to set it to 13V) for the amplifier power supply.

Best regards,