I have a fundamental question about operation that I was not able to glean from the datasheet. I want to understand the relationship to VSYS and PMID for the 4 following cases:
1) If powered from 5V on VBUS and VBAT = 3.8V: PMID = 5V (follows VBUS) and VSYS = ~3.8V (follows battery)
2) If powered from 5V on VBUS and VBAT = 3.0V: PMID = 5V (follows VBUS) and VSYS = ~3.5V (boost to Vsys_min)
3) If VBUS is not present and VBAT = 3.8V: PMID = 5.1V (boost) and VSYS = ~3.8V (follows battery)
4) If VBUS is not present and VBAT = 3.0V: PMID = 5.1V (boost) and VSYS = ??? (does it follow the battery or maintain the 3.5V Vsys_min)
If case 4), can the device boost both PMID and VSYS from a battery below Vsys_min?