This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CSD18540Q5B: Looking for pin to pin replacement mosfet like CSD18540Q5B

Expert 1035 points

Replies: 3

Views: 38

Part Number: CSD18540Q5B

Hi everyone,

I'm using NVMTS0D4N04C mosfet for my application, but I need to change this mosfet with pin to pin mosfet. I would like to use the CSD18540Q5B mosfet but it is not pin to pin. If you have similar product, please let me know.

Thanks!

  • Hi Ali,

    Thanks for your interest in TI FETs. Unfortunately, we do not make any FETs in the same 8 x 8mm (POWER 88) package. You would need to change your board layout to accommodate either a 5 x 6mm SON or D2PAK device.

    Best Regards,

    John Wallace

    MOSFET technical information on ti.com here

  • In reply to John Wallace1:

    Hi John, 

    Thank you for the reply. If you have any part number for pin to pin connection, I would like to use it for my PCB. Then I can change the layout for revision 2. Same footprint is not important for my test.

  • In reply to alikaan:

    Hi Ali,

    Thanks again for your interest in TI FETs. I did a search and unfortunately TI does not make any devices (FETs or otherwise) in the same package as the NVMTS0D4N04C. The closest we have is a 5x6mm SON package such as the CSD18540Q5B. Our lowest rds(on) 40V NFET is the CSD18510Q5B in 5x6mm SON package.

    Best Regards,

    John Wallace

    MOSFET technical information on ti.com here

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.