Hi TI Support,
I plan to use a common mode choke to filter the incoming 24V power. The amperage rating of the choke is less than the expected draw from the loads on multiple TPS4H160 power switches, so I would like to supply the TPS4H160 switches with the non-filtered incoming 24V supply. But since the grounds of the MCU and TPS4H160 circuits would not be exactly the same, I am wondering if it will work, and if there are any precautions I need to take. At DC, the grounds are essentially the same since the DC resistance of the common mode choke is about 65 mOhms per coil. But there is significant impedance to AC waveforms. The inductance of each coil is about 470 uH.
Here is a simplified schematic showing the circuit with the grounds and supplies. I've shown example circuits for both the A and B versions of the TPS4H160.
In particular, please consider the following questions:
1. Since the frequency of switching is very low, will the TPS4H160 behave properly given the ground differences I've outlined? The rising edge of the control input is an AC waveform, but only for the duration of the leading and trailing edges. The circuit should stabilize before the next edge occurs. Will the inductance of the choke cause problems with overshoot and undershoot? If so, can this be mitigated by slowing down the edges, or are there components I can add to clamp them?
2. Are there any issues with +5V and its ground supplying DIAG_EN, THER, SEH/SEL, or the fault LEDs?
3. The B version has the additional issue of the MCU accurately measuring the Current Sense (CS pin) output. Is the CS output a current source? If so, would it be permissible to connect that output to the MCU's ground? If it is truly a current source, wouldn't the voltage dropped across the resistor be accurate even though the grounds are dissimilar? But since the grounds are connected to each other via a 470 uH inductor, I assume the frequency response would be affected and the inductance could affect the current source circuit.
If this is a dicey configuration, I won't do it and I will need to isolate the circuit. Or I could use a much beefier common mode choke and supply the TPS4H160 drivers with filtered 24V.
Thank you very much for the help.
Regards,
Greg