Other Parts Discussed in Thread: INA139, TL431, UCC25600
Hi,
I am working on a project that will be using the UCC29002 on a 24V power stage. Referring from the datasheet, figure 5 suggests a circuit configuration for high voltage application, however this recommended circuit is not applicable in my project because the 24V power stage shares the same ground with the 5.1V and 3.3V power stages. That means I have to place the sense resistor along the positive 24V rail and I need to do some workaround to maintain safe voltage levels on the CS+, CS- and ADJ pins. I have a couple of questions:
1. Can you give me a recommendation on a circuit configuration that will input safe voltage levels on CS+ and CS- from a sense resistor along the positive 24V rail? I am planning to insert the INA139 current shunt monitor across the sense resistor and make its output enter the current sense amplifier of the UCC29002 in non-inverting amplifier configuration. Is this a good idea?
2. The 24V power stage has a feedback circuit based on TL431 and an optocoupler combination. I would like to ask on how to effectively attach the ADJ pin on this kind of high voltage feedback circuit. Is there a way to do this?
Thanks,
Chester