This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 71
Part Number: UCC28019A
Hello E2E,
Our customer are considering using the UCC28019A for AC24Vin block on during to developing equipment. I obtained the capture of schematic from them. Could TI engineers check this schematic?
Best regards,ACGUY
Hello ACGUY,
It is unusual to use the smart diode controller LM74670 and synchronous rectification on a pfc stage.The very low input impedance into the large bus capacitance may cause a very large inrush current at start up and failure of a componentunless some inrush protection is added to the pfc.I think a startup resistor is required to pre charge the output capacitors.Normally you would short out this resistor after a pre determined time and then enable the pfc.The design should give excellent efficiency but it needs to be protected from transient conditions.
Im not sure what value of inductance is used but it needs to be 160uH or greater for this application.
Those are my only comments.
In reply to John Griffin1:
Hello John,
Thank you for your comment. About settings RC value, does this schematic have any mistake?
Best regards,
ACGUY
In reply to ACGUY:
I did not see an error in any component value or have any more suggestions or comments.
Regards
John