The calculation formula of ΔB is described in P40 of the data sheet. (8.2.2.2.3-2)
Is this formula true for all output conditions?
For example, consider a rated output of 192W (32V, 6A).
In that case, I think I should enter 192 in Po (fl).
As a result, I think Im +, ΔB, Fsw, D, etc. will be calculated.
If I want to know Im +, ΔB, Fsw, D under the condition of 14W (1 / 8Po (fl)), should I input 14 to Po (fl)?
Also, can I think of it as a formula that can be applied to both AAM and ABM?
Also, please advise us about the air gap of the transformer used for the evaluation board.
When I use the small core (RM8), the gap is over 1mm. If the inductance value is set to about 30uH, it will be about 1.5mm.
I'm worried that it's too big, but is it acceptable for a small high-frequency flyback? (Please tell us the common air gap value.
If it is a normal flyback (100 kHz or less), I will redesign it if it becomes 1 mm or more)
However, if the leakage inductance is intentionally used in this circuit method, is it OK to consider a large gap value?
There is a concern that the gap exceeds 1 mm, but if there is a tendency peculiar to this circuit, prototype it and evaluate it.
Of course, if you recommend a gap of 1 mm or less, redesign. (Increase the core size, etc.)
B.R.Tak