Dear,
I would like to use a TPS2120 as a relay that would have a 17 V on the first input (In1) and that would be not connected on the second input (In2).
I will use the SEL pin to switch between both inputs.
In a first time would like that you confirme me it could be done?
In a second time I would like to know if the TPS2120 could perform an at least 3500 V/s slew rate (up to 17000 V/s max) for a max current of 32 mA and a load capacitor from 1 to 10 pF?
Best regards,
Romain