Team,
For the below flyback spec:
185/265VAC / 50hz -> 10VDC @ 3.2A
The two main requirements are: low cost and small size
1) In order to reduce size:
Looking at datasheet page 14: Is there a way with UCC28C44 to use a transformer with only NP and NS (and no NA winding)?
Or is NA mandatory to start up and power the UCC28C44?
2) If 1) can not be done what do you advise to optimize the size of the solution?
Do you have tips to reduce the size of the transformer for this use case?
Thanks in advance!
A.