I designed in the 2.5, 3.0, and 3.3 V versions of this regulator without noticing the awful load transient response (fig 19 in the data sheet). This has become a problem in the prototype. Is there a drop-in replacement for this family with better specs? A small amount of rework would be acceptable too. I need the three voltages I mentioned, with a 5 V input. Super low power is not important, but I do need at least 150 mA output.
Thanks for any help!