Hi,
I am designing a 7V-16V Vin to 5.1V Vout @ 3.5A regulator based on the TPS565201. There is a second power source in the design that may be occasionally connected. It would supply 5V at the output of the TPS565201. Is the TPS565201 okay to use under the following conditions (all of these conditions assume a second source providing 5V at output):
1. Vin = 0V, EN = 0V, Vout = 5V
2. Vin = 5V, EN = 0V, Vout = 5V
3. Vin = 15V, EN = 0V, Vout = 5V
Thanks in advance,
Josh