This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5575: LM5575 Simulation by PSPICE

Part Number: LM5575

Good afternoon,

I have to simulate the LM5575 by PSPICE. I need 3.3V at the output. the input voltage is 24V. I have doubt for filling the steady part which is in PSPICE model. I've already put -1.5. The problem is that the simulation takes too long time and it shows me 24V at the output. and that means that the chip doesn't work.Any suggestion?

Sincerely

Farzaneh