Other Parts Discussed in Thread: TPS54383, , TPS54386EVM
Hi,
The datasheet of TPS5438x stated that the input range is 4.5V to 28V and the maximum output current is 3A. However, the spec of the EVM stated that the input range is 9.6V to 13.2V and the maximum output current is 2A.
My design requirement is 24V input, 3.3V and 5V output with 3A each.
Can you let me know if this IC is suitable for my design requirement? If yes, what would I have to change in the EVM circuit in order to meet my design requirements?
Thanks,
Jeff