This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74901: Can Vbias connected to Vin at 2.5V?

Part Number: TPS74901
Other Parts Discussed in Thread: TPS740

Hi, 

I am using the TPS74091 to generate 1.8V from 2.5V. Can I connect Vbias to the same 2.5V as Vin? Or it has to be 1.75V larger than 1.8V? 

Thank you.