Hi,
I am currently working on an isolated flyback converter design
Vin: typ. 24V, 20V - 30V min/max
Vout: 12V, 3A max
using the following WEBENCH design and design guide:
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=71FCBC144E2150BF
http://www.ti.com/lit/an/snva866/snva866.pdf
My question is: Can i use a second primary winding/ auxiliary winding as an output on my primary side? I would need 5V @ 150mA max.
In the design guide it is not really mentioned how they ensured the maximum current rating on the aux winding nor the expected voltage ripple on the aux winding.
Best regards,
Jan