Hi does TI provide driver sample C code for PMID bq25155?
My company would like to use a driver sample code as a reference to develop our own driver for Nordic embedded system.
Thanks. Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi does TI provide driver sample C code for PMID bq25155?
My company would like to use a driver sample code as a reference to develop our own driver for Nordic embedded system.
Thanks. Regards.
Hello,
I've attached a driver.
// SPDX-License-Identifier: GPL-2.0 // BQ2515X Battery Charger Driver // Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/ #include <linux/err.h> #include <linux/i2c.h> #include <linux/init.h> #include <linux/interrupt.h> #include <linux/kernel.h> #include <linux/module.h> #include <linux/of_device.h> #include <linux/gpio/consumer.h> #include <linux/power_supply.h> #include <linux/regmap.h> #include <linux/types.h> #define BQ2515X_MANUFACTURER "Texas Instruments" #define BQ2515X_STAT0 0x00 #define BQ2515X_STAT1 0x01 #define BQ2515X_STAT2 0x02 #define BQ2515X_FLAG0 0x03 #define BQ2515X_FLAG1 0x04 #define BQ2515X_FLAG2 0x05 #define BQ2515X_FLAG3 0x06 #define BQ2515X_MASK0 0x07 #define BQ2515X_MASK1 0x08 #define BQ2515X_MASK2 0x09 #define BQ2515X_MASK3 0x0a #define BQ2515X_VBAT_CTRL 0x12 #define BQ2515X_ICHG_CTRL 0x13 #define BQ2515X_PCHRGCTRL 0x14 #define BQ2515X_TERMCTRL 0x15 #define BQ2515X_BUVLO 0x16 #define BQ2515X_CHARGERCTRL0 0x17 #define BQ2515X_CHARGERCTRL1 0x18 #define BQ2515X_ILIMCTRL 0x19 #define BQ2515X_LDOCTRL 0x1d #define BQ2515X_MRCTRL 0x30 #define BQ2515X_ICCTRL0 0x35 #define BQ2515X_ICCTRL1 0x36 #define BQ2515X_ICCTRL2 0x37 #define BQ2515X_ADCCTRL0 0x40 #define BQ2515X_ADCCTRL1 0x41 #define BQ2515X_ADC_VBAT_M 0x42 #define BQ2515X_ADC_VBAT_L 0x43 #define BQ2515X_ADC_TS_M 0x44 #define BQ2515X_ADC_TS_L 0x45 #define BQ2515X_ADC_ICHG_M 0x46 #define BQ2515X_ADC_ICHG_L 0x47 #define BQ2515X_ADC_ADCIN_M 0x48 #define BQ2515X_ADC_ADCIN_L 0x49 #define BQ2515X_ADC_VIN_M 0x4a #define BQ2515X_ADC_VIN_L 0x4b #define BQ2515X_ADC_PMID_M 0x4c #define BQ2515X_ADC_PMID_L 0x4d #define BQ2515X_ADC_IIN_M 0x4e #define BQ2515X_ADC_IIN_L 0x4f #define BQ2515X_ADC_COMP1_M 0x52 #define BQ2515X_ADC_COMP1_L 0X53 #define BQ2515X_ADC_COMP2_M 0X54 #define BQ2515X_ADC_COMP2_L 0x55 #define BQ2515X_ADC_COMP3_M 0x56 #define BQ2515X_ADC_COMP3_L 0x57 #define BQ2515X_ADC_READ_EN 0x58 #define BQ2515X_TS_FASTCHGCTRL 0x61 #define BQ2515X_TS_COLD 0x62 #define BQ2515X_TS_COOL 0x63 #define BQ2515X_TS_WARM 0x64 #define BQ2515X_TS_HOT 0x65 #define BQ2515X_DEVICE_ID 0x6f #define BQ2515X_DEFAULT_ICHG_UA 10000 #define BQ25150_DEFAULT_ILIM_UA 100000 #define BQ25155_DEFAULT_ILIM_UA 500000 #define BQ2515X_DEFAULT_VBAT_REG_UV 4200000 #define BQ2515X_DEFAULT_IPRECHARGE_UA 2500 #define BQ2515X_DIVISOR 65536 #define BQ2515X_VBAT_BASE_VOLT 3600000 #define BQ2515X_VBAT_REG_MAX 4600000 #define BQ2515X_VBAT_REG_MIN 3600000 #define BQ2515X_VBAT_STEP_UV 10000 #define BQ2515X_UV_FACTOR 1000000 #define BQ2515X_ICHG_DIVISOR 52429 #define BQ2515X_ICHG_CURR_STEP_THRESH_UA 318750 #define BQ2515X_ICHG_MIN_UA 0 #define BQ2515X_ICHG_MAX_UA 500000 #define BQ2515X_ICHG_RNG_1B0_UA 1250 #define BQ2515X_ICHG_RNG_1B1_UA 2500 #define BQ2515X_VLOWV_SEL_1B0_UV 3000000 #define BQ2515X_VLOWV_SEL_1B1_UV 2800000 #define BQ2515X_PRECHRG_ICHRG_RNGE_1875_UA 18750 #define BQ2515X_PRECHRG_ICHRG_RNGE_3750_UA 37500 #define BQ2515X_TWAKE2_MIN_US 1700000 #define BQ2515X_TWAKE2_MAX_US 2300000 #define BQ2515X_ILIM_150MA 0x2 #define BQ2515X_ILIM_MASK 0x7 #define BQ2515X_HEALTH_MASK 0xf #define BQ2515X_ICHGRNG_MASK 0x80 #define BQ2515X_STAT0_MASK 0x0f #define BQ2515X_STAT1_MASK 0x1f #define BQ2515X_PRECHARGE_MASK 0x1f #define BQ2515X_TS_HOT_STAT BIT(0) #define BQ2515X_TS_WARM_STAT BIT(1) #define BQ2515X_TS_COOL_STAT BIT(2) #define BQ2515X_TS_COLD_STAT BIT(3) #define BQ2515X_SAFETY_TIMER_EXP BIT(5) #define BQ2515X_VIN_GOOD BIT(0) #define BQ2515X_CHRG_DONE BIT(5) #define BQ2515X_CV_CHRG_MODE BIT(6) #define BQ2515X_VIN_OVP_FAULT_STAT BIT(7) #define BQ2515X_WATCHDOG_DISABLE BIT(4) #define BQ2515X_ICHARGE_RANGE BIT(7) #define BQ2515X_VLOWV_SEL BIT(5) #define BQ2515X_CHARGER_DISABLE BIT(0) #define BQ2515X_HWRESET_14S_WD BIT(1) static const int bq2515x_ilim_lvl_values[] = { 50000, 100000, 150000, 200000, 300000, 400000, 500000, 600000 }; /** * struct bq2515x_init_data - * @icgh: fast charge current * @vreg: charge voltage * @ilim: input current limit * @iprecharge: precharge current */ struct bq2515x_init_data { int ichg; int vreg; int ilim; int iprecharge; }; enum bq2515x_id { BQ25150, BQ25155, BQ21061, }; /** * struct bq2515x_device - * @mains: mains properties * @battery: battery properties * @client: i2c client structure * @regmap: register map structure * @dev: device structure * @lock: thread lock structure * @id: enumeration of device ids * * @reset_gpio: manual reset (MR) pin * @lp_gpio: low power mode pin * @ac_detect_gpio: power good (PG) pin * @ce_gpio: charge enable (CE) pin * * @model_name: string value describing device model * @device_id: value of device_id * @mains_online: boolean value indicating power supply online * * @bq2515x_init_data init_data: charger initialization data structure */ struct bq2515x_device { struct power_supply *mains; struct power_supply *battery; struct i2c_client *client; struct regmap *regmap; struct device *dev; struct mutex lock; enum bq2515x_id id; struct gpio_desc *reset_gpio; struct gpio_desc *lp_gpio; struct gpio_desc *ac_detect_gpio; struct gpio_desc *ce_gpio; char model_name[I2C_NAME_SIZE]; int device_id; bool mains_online; struct bq2515x_init_data init_data; }; static struct reg_default bq25150_reg_defs[] = { {BQ2515X_FLAG0, 0x0}, {BQ2515X_FLAG1, 0x0}, {BQ2515X_FLAG2, 0x0}, {BQ2515X_FLAG3, 0x0}, {BQ2515X_MASK0, 0x0}, {BQ2515X_MASK1, 0x0}, {BQ2515X_MASK2, 0x71}, {BQ2515X_MASK3, 0x0}, {BQ2515X_VBAT_CTRL, 0x3C}, {BQ2515X_ICHG_CTRL, 0x8}, {BQ2515X_PCHRGCTRL, 0x2}, {BQ2515X_TERMCTRL, 0x14}, {BQ2515X_BUVLO, 0x0}, {BQ2515X_CHARGERCTRL0, 0x82}, {BQ2515X_CHARGERCTRL1, 0x42}, {BQ2515X_ILIMCTRL, 0x1}, {BQ2515X_LDOCTRL, 0xB0}, {BQ2515X_MRCTRL, 0x2A}, {BQ2515X_ICCTRL0, 0x10}, {BQ2515X_ICCTRL1, 0x0}, {BQ2515X_ICCTRL2, 0x0}, {BQ2515X_ADCCTRL0, 0x2}, {BQ2515X_ADCCTRL1, 0x40}, {BQ2515X_ADC_COMP1_M, 0x23}, {BQ2515X_ADC_COMP1_L, 0x20}, {BQ2515X_ADC_COMP2_M, 0x38}, {BQ2515X_ADC_COMP2_L, 0x90}, {BQ2515X_ADC_COMP3_M, 0x0}, {BQ2515X_ADC_COMP3_L, 0x0}, {BQ2515X_ADC_READ_EN, 0x0}, {BQ2515X_TS_FASTCHGCTRL, 0x34}, {BQ2515X_TS_COLD, 0x7C}, {BQ2515X_TS_COOL, 0x6D}, {BQ2515X_TS_WARM, 0x38}, {BQ2515X_TS_HOT, 0x27}, {BQ2515X_DEVICE_ID, 0x20}, }; static struct reg_default bq25155_reg_defs[] = { {BQ2515X_FLAG0, 0x0}, {BQ2515X_FLAG1, 0x0}, {BQ2515X_FLAG2, 0x0}, {BQ2515X_FLAG3, 0x0}, {BQ2515X_MASK0, 0x0}, {BQ2515X_MASK1, 0x0}, {BQ2515X_MASK2, 0x71}, {BQ2515X_MASK3, 0x0}, {BQ2515X_VBAT_CTRL, 0x3C}, {BQ2515X_ICHG_CTRL, 0x8}, {BQ2515X_PCHRGCTRL, 0x2}, {BQ2515X_TERMCTRL, 0x14}, {BQ2515X_BUVLO, 0x0}, {BQ2515X_CHARGERCTRL0, 0x82}, {BQ2515X_CHARGERCTRL1, 0xC2}, {BQ2515X_ILIMCTRL, 0x6}, {BQ2515X_LDOCTRL, 0xB0}, {BQ2515X_MRCTRL, 0x2A}, {BQ2515X_ICCTRL0, 0x10}, {BQ2515X_ICCTRL1, 0x0}, {BQ2515X_ICCTRL2, 0x40}, {BQ2515X_ADCCTRL0, 0x2}, {BQ2515X_ADCCTRL1, 0x40}, {BQ2515X_ADC_COMP1_M, 0x23}, {BQ2515X_ADC_COMP1_L, 0x20}, {BQ2515X_ADC_COMP2_M, 0x38}, {BQ2515X_ADC_COMP2_L, 0x90}, {BQ2515X_ADC_COMP3_M, 0x0}, {BQ2515X_ADC_COMP3_L, 0x0}, {BQ2515X_ADC_READ_EN, 0x0}, {BQ2515X_TS_FASTCHGCTRL, 0x34}, {BQ2515X_TS_COLD, 0x7C}, {BQ2515X_TS_COOL, 0x6D}, {BQ2515X_TS_WARM, 0x38}, {BQ2515X_TS_HOT, 0x27}, {BQ2515X_DEVICE_ID, 0x35}, }; static struct reg_default bq21061_reg_defs[] = { {BQ2515X_FLAG0, 0x0}, {BQ2515X_FLAG1, 0x0}, {BQ2515X_FLAG2, 0x0}, {BQ2515X_FLAG3, 0x0}, {BQ2515X_MASK0, 0x0}, {BQ2515X_MASK1, 0x0}, {BQ2515X_MASK2, 0x71}, {BQ2515X_MASK3, 0x0}, {BQ2515X_VBAT_CTRL, 0x3C}, {BQ2515X_ICHG_CTRL, 0x8}, {BQ2515X_PCHRGCTRL, 0x2}, {BQ2515X_TERMCTRL, 0x14}, {BQ2515X_BUVLO, 0x0}, {BQ2515X_CHARGERCTRL0, 0x82}, {BQ2515X_CHARGERCTRL1, 0xC2}, {BQ2515X_ILIMCTRL, 0x6}, {BQ2515X_LDOCTRL, 0xB0}, {BQ2515X_MRCTRL, 0x2A}, {BQ2515X_ICCTRL0, 0x10}, {BQ2515X_ICCTRL1, 0x0}, {BQ2515X_ICCTRL2, 0x40}, {BQ2515X_TS_FASTCHGCTRL, 0x34}, {BQ2515X_TS_COLD, 0x7C}, {BQ2515X_TS_COOL, 0x6D}, {BQ2515X_TS_WARM, 0x38}, {BQ2515X_TS_HOT, 0x27}, {BQ2515X_DEVICE_ID, 0x3A}, }; static bool bq2515x_is_ps_online(struct bq2515x_device *bq2515x) { return bq2515x->mains_online; } static int bq2515x_wake_up(struct bq2515x_device *bq2515x) { int ret; int val; /* Read the STAT register if we can read it then the device is out * of ship mode. If the register cannot be read then attempt to wake * it up and enable the ADC. */ ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &val); if (!ret) return ret; /* Need to toggle LP and bring device out of ship mode. The device * will exit the ship mode when the MR pin is held low for at least * t_WAKE2 as shown in section 8.3.7.1 of the datasheet. */ if (bq2515x->lp_gpio) gpiod_set_value_cansleep(bq2515x->lp_gpio, 0); if (bq2515x->lp_gpio) { gpiod_set_value_cansleep(bq2515x->reset_gpio, 0); usleep_range(BQ2515X_TWAKE2_MIN_US, BQ2515X_TWAKE2_MAX_US); gpiod_set_value_cansleep(bq2515x->reset_gpio, 1); } return regmap_write(bq2515x->regmap, BQ2515X_ADC_READ_EN, BIT(3)); } static int bq2515x_update_ps_status(struct bq2515x_device *bq2515x) { bool dc = false; unsigned int val; int ret; if (bq2515x->ac_detect_gpio) val = gpiod_get_value_cansleep(bq2515x->ac_detect_gpio); else { ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &val); if (ret < 0) return ret; } dc = val & BQ2515X_VIN_GOOD; ret = bq2515x->mains_online != dc; bq2515x->mains_online = dc; return ret; } static int bq2515x_disable_watchdog_timers(struct bq2515x_device *bq2515x) { int ret; ret = regmap_update_bits(bq2515x->regmap, BQ2515X_CHARGERCTRL0, BQ2515X_WATCHDOG_DISABLE, BQ2515X_WATCHDOG_DISABLE); if (ret < 0) return ret; return regmap_update_bits(bq2515x->regmap, BQ2515X_ICCTRL2, BQ2515X_HWRESET_14S_WD, 0); } static int bq2515x_get_battery_voltage_now(struct bq2515x_device *bq2515x) { int ret; int vbat_msb; int vbat_lsb; uint32_t vbat_measurement; if (!bq2515x_is_ps_online(bq2515x)) bq2515x_wake_up(bq2515x); ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_VBAT_M, &vbat_msb); if (ret) return ret; ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_VBAT_L, &vbat_lsb); if (ret) return ret; vbat_measurement = (vbat_msb << 8) | vbat_lsb; return vbat_measurement * (BQ2515X_UV_FACTOR / BQ2515X_DIVISOR) * 6; } static int bq2515x_get_battery_current_now(struct bq2515x_device *bq2515x) { int ret; int ichg_msb; int ichg_lsb; uint32_t ichg_measurement; u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA; unsigned int ichg_reg_code, reg_code; unsigned int icharge_range = 0, pchrgctrl; unsigned int buvlo, vlowv_sel, vlowv = BQ2515X_VLOWV_SEL_1B0_UV; if (!bq2515x_is_ps_online(bq2515x)) return -ENODATA; ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_ICHG_M, &ichg_msb); if (ret < 0) return ret; ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_ICHG_L, &ichg_lsb); if (ret < 0) return ret; ichg_measurement = (ichg_msb << 8) | ichg_lsb; ret = regmap_read(bq2515x->regmap, BQ2515X_BUVLO, &buvlo); if (ret < 0) return ret; vlowv_sel = buvlo & BQ2515X_VLOWV_SEL; if (vlowv_sel) vlowv = BQ2515X_VLOWV_SEL_1B1_UV; if (bq2515x_get_battery_voltage_now(bq2515x) < vlowv) { ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl); if (ret < 0) return ret; reg_code = pchrgctrl & BQ2515X_PRECHARGE_MASK; } else { ret = regmap_read(bq2515x->regmap, BQ2515X_ICHG_CTRL, &ichg_reg_code); if (ret < 0) return ret; reg_code = ichg_reg_code; } ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl); if (ret < 0) return ret; icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE; if (icharge_range) ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA; return reg_code * (ichg_multiplier * ichg_measurement / BQ2515X_ICHG_DIVISOR); } static bool bq2515x_get_charge_disable(struct bq2515x_device *bq2515x) { int ret; int ce_pin = 0; int icctrl2; int charger_disable; if (bq2515x->ce_gpio) ce_pin = gpiod_get_value_cansleep(bq2515x->ce_gpio); ret = regmap_read(bq2515x->regmap, BQ2515X_ICCTRL2, &icctrl2); if (ret < 0) return ret; charger_disable = icctrl2 & BQ2515X_CHARGER_DISABLE; if (charger_disable || ce_pin) return true; return false; } static int bq2515x_set_charge_disable(struct bq2515x_device *bq2515x, int val) { if (bq2515x->ce_gpio) gpiod_set_value_cansleep(bq2515x->ce_gpio, val); return regmap_update_bits(bq2515x->regmap, BQ2515X_ICCTRL2, BQ2515X_CHARGER_DISABLE, val); } static int bq2515x_get_const_charge_current(struct bq2515x_device *bq2515x) { int ret; u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA; unsigned int ichg_reg_code; unsigned int pchrgctrl; unsigned int icharge_range; ret = regmap_read(bq2515x->regmap, BQ2515X_ICHG_CTRL, &ichg_reg_code); if (ret < 0) return ret; ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl); if (ret < 0) return ret; icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE; if (icharge_range) ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA; return ichg_reg_code * ichg_multiplier; } static int bq2515x_set_const_charge_current(struct bq2515x_device *bq2515x, int val) { int ret; unsigned int ichg_reg_code; u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA; unsigned int icharge_range = 0; if (val > BQ2515X_ICHG_MAX_UA || val < BQ2515X_ICHG_MIN_UA) return -EINVAL; if (val > BQ2515X_ICHG_CURR_STEP_THRESH_UA) { ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA; icharge_range = BQ2515X_ICHARGE_RANGE; } bq2515x_set_charge_disable(bq2515x, 1); ret = regmap_update_bits(bq2515x->regmap, BQ2515X_PCHRGCTRL, BQ2515X_ICHARGE_RANGE, icharge_range); if (ret < 0) return ret; ichg_reg_code = val / ichg_multiplier; ret = regmap_write(bq2515x->regmap, BQ2515X_ICHG_CTRL, ichg_reg_code); if (ret < 0) return ret; return bq2515x_set_charge_disable(bq2515x, 0); } static int bq2515x_get_precharge_current(struct bq2515x_device *bq2515x) { int ret; unsigned int pchrgctrl; unsigned int icharge_range; u16 precharge_multiplier = BQ2515X_ICHG_RNG_1B0_UA; unsigned int precharge_reg_code; ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl); if (ret < 0) return ret; icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE; if (icharge_range) precharge_multiplier = BQ2515X_ICHG_RNG_1B1_UA; precharge_reg_code = pchrgctrl & BQ2515X_PRECHARGE_MASK; return precharge_reg_code * precharge_multiplier; } static int bq2515x_set_precharge_current(struct bq2515x_device *bq2515x, int val) { int ret; unsigned int pchrgctrl; unsigned int icharge_range; unsigned int precharge_reg_code; u16 precharge_multiplier = BQ2515X_ICHG_RNG_1B0_UA; u16 precharge_max_ua = BQ2515X_PRECHRG_ICHRG_RNGE_1875_UA; ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl); if (ret < 0) return ret; icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE; if (icharge_range) { precharge_max_ua = BQ2515X_PRECHRG_ICHRG_RNGE_3750_UA; precharge_multiplier = BQ2515X_ICHG_RNG_1B1_UA; } if (val > precharge_max_ua || val < BQ2515X_ICHG_MIN_UA) return -EINVAL; precharge_reg_code = val / precharge_multiplier; ret = bq2515x_set_charge_disable(bq2515x, 1); if (ret < 0) return ret; ret = regmap_update_bits(bq2515x->regmap, BQ2515X_PCHRGCTRL, BQ2515X_PRECHARGE_MASK, precharge_reg_code); if (ret < 0) return ret; return bq2515x_set_charge_disable(bq2515x, 0); } static int bq2515x_charging_status(struct bq2515x_device *bq2515x, union power_supply_propval *val) { bool status0_no_fault; bool status1_no_fault; bool ce_status; bool charge_done; unsigned int status; int ret; if (!bq2515x_is_ps_online(bq2515x)) { val->intval = POWER_SUPPLY_STATUS_DISCHARGING; return 0; } ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &status); if (ret) return ret; /** * The code block below is used to determine if any faults from the * STAT0 register are disbaling charging or if the charge has completed * according to the CHARGE_DONE_STAT bit. */ if (((status & BQ2515X_STAT0_MASK) == true) & ((status & BQ2515X_CHRG_DONE) == false)) { status0_no_fault = true; charge_done = false; } else if (status & BQ2515X_CHRG_DONE) { charge_done = true; status0_no_fault = false; } else { status0_no_fault = false; charge_done = false; } ret = regmap_read(bq2515x->regmap, BQ2515X_STAT1, &status); if (ret) return ret; /** *The code block below is used to determine if any faults from the * STAT1 register are disbaling charging */ if ((status & BQ2515X_STAT1_MASK) == false) status1_no_fault = true; else status1_no_fault = false; ce_status = (!bq2515x_get_charge_disable(bq2515x)); /** *If there are no faults and charging is enabled, then status is *charging. Otherwise, if charging is complete, then status is full. *Otherwise, if a fault exists or charging is disbaled, then status is *not charging */ if (status0_no_fault & status1_no_fault & ce_status) val->intval = POWER_SUPPLY_STATUS_CHARGING; else if (charge_done) val->intval = POWER_SUPPLY_STATUS_FULL; else if (!(status0_no_fault & status1_no_fault & ce_status)) val->intval = POWER_SUPPLY_STATUS_NOT_CHARGING; return ret; } static int bq2515x_get_batt_reg(struct bq2515x_device *bq2515x) { int vbat_reg_code; int ret; ret = regmap_read(bq2515x->regmap, BQ2515X_VBAT_CTRL, &vbat_reg_code); if (ret) return ret; return BQ2515X_VBAT_BASE_VOLT + vbat_reg_code * BQ2515X_VBAT_STEP_UV; } static int bq2515x_set_batt_reg(struct bq2515x_device *bq2515x, int val) { int vbat_reg_code; if (val > BQ2515X_VBAT_REG_MAX || val < BQ2515X_VBAT_REG_MIN) return -EINVAL; vbat_reg_code = (val - BQ2515X_VBAT_BASE_VOLT) / BQ2515X_VBAT_STEP_UV; return regmap_write(bq2515x->regmap, BQ2515X_VBAT_CTRL, vbat_reg_code); } static int bq2515x_get_ilim_lvl(struct bq2515x_device *bq2515x) { int ret; int ilimctrl; ret = regmap_read(bq2515x->regmap, BQ2515X_ILIMCTRL, &ilimctrl); if (ret) return ret; return bq2515x_ilim_lvl_values[ilimctrl & BQ2515X_ILIM_MASK]; } static int bq2515x_set_ilim_lvl(struct bq2515x_device *bq2515x, int val) { int i; for (i = 0; i < ARRAY_SIZE(bq2515x_ilim_lvl_values); i++) { if (val == bq2515x_ilim_lvl_values[i]) break; if (val > bq2515x_ilim_lvl_values[i - 1] && val < bq2515x_ilim_lvl_values[i]) { if (val - bq2515x_ilim_lvl_values[i - 1] < bq2515x_ilim_lvl_values[i] - val) { i = i - 1; break; } } } return regmap_write(bq2515x->regmap, BQ2515X_ILIMCTRL, i); } static int bq2515x_power_supply_property_is_writeable(struct power_supply *psy, enum power_supply_property prop) { switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: return true; default: return false; } } static int bq2515x_charger_get_health(struct bq2515x_device *bq2515x, union power_supply_propval *val) { int health = POWER_SUPPLY_HEALTH_GOOD; int ret; unsigned int stat1; unsigned int flag3; if (!bq2515x_is_ps_online(bq2515x)) bq2515x_wake_up(bq2515x); ret = regmap_read(bq2515x->regmap, BQ2515X_FLAG3, &flag3); if (ret) return ret; if (flag3 & BQ2515X_SAFETY_TIMER_EXP) { health = POWER_SUPPLY_HEALTH_SAFETY_TIMER_EXPIRE; goto ret_health; } if (stat1 & BQ2515X_VIN_OVP_FAULT_STAT) { health = POWER_SUPPLY_HEALTH_OVERVOLTAGE; goto ret_health; } ret = regmap_read(bq2515x->regmap, BQ2515X_STAT1, &stat1); if (ret) return ret; if (stat1 & BQ2515X_HEALTH_MASK) { switch (stat1 & BQ2515X_HEALTH_MASK) { case BQ2515X_TS_HOT_STAT: health = POWER_SUPPLY_HEALTH_HOT; break; case BQ2515X_TS_WARM_STAT: health = POWER_SUPPLY_HEALTH_WARM; break; case BQ2515X_TS_COOL_STAT: health = POWER_SUPPLY_HEALTH_COOL; break; case BQ2515X_TS_COLD_STAT: health = POWER_SUPPLY_HEALTH_COLD; break; default: health = POWER_SUPPLY_HEALTH_UNKNOWN; break; } } goto ret_health; ret_health: val->intval = health; return 0; } static int bq2515x_mains_set_property(struct power_supply *psy, enum power_supply_property prop, const union power_supply_propval *val) { struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy); int ret; switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2515x_set_ilim_lvl(bq2515x, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2515x_set_batt_reg(bq2515x, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2515x_set_const_charge_current(bq2515x, val->intval); break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2515x_set_precharge_current(bq2515x, val->intval); break; default: return -EINVAL; } return ret; } static int bq2515x_mains_get_property(struct power_supply *psy, enum power_supply_property prop, union power_supply_propval *val) { struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy); int ret = 0; switch (prop) { case POWER_SUPPLY_PROP_ONLINE: val->intval = bq2515x->mains_online; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2515x_get_const_charge_current(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2515x_get_precharge_current(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2515x_get_ilim_lvl(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2515x_get_batt_reg(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_MODEL_NAME: val->strval = bq2515x->model_name; break; case POWER_SUPPLY_PROP_MANUFACTURER: val->strval = BQ2515X_MANUFACTURER; break; case POWER_SUPPLY_PROP_VOLTAGE_MAX: val->intval = BQ2515X_VBAT_REG_MAX; break; case POWER_SUPPLY_PROP_VOLTAGE_MIN: val->intval = BQ2515X_VBAT_REG_MIN; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX: val->intval = BQ2515X_ICHG_MAX_UA; break; default: return -EINVAL; } return ret; } static int bq2515x_battery_get_property(struct power_supply *psy, enum power_supply_property prop, union power_supply_propval *val) { struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy); int ret; ret = bq2515x_update_ps_status(bq2515x); if (ret < 0) return ret; switch (prop) { case POWER_SUPPLY_PROP_STATUS: if (!bq2515x_is_ps_online(bq2515x)) { val->intval = POWER_SUPPLY_STATUS_DISCHARGING; break; } ret = bq2515x_charging_status(bq2515x, val); break; case POWER_SUPPLY_PROP_VOLTAGE_NOW: ret = bq2515x_get_battery_voltage_now(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CURRENT_NOW: ret = bq2515x_get_battery_current_now(bq2515x); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_HEALTH: ret = bq2515x_charger_get_health(bq2515x, val); if (ret) val->intval = POWER_SUPPLY_HEALTH_UNKNOWN; break; default: return -EINVAL; } return 0; } static enum power_supply_property bq2515x_battery_properties[] = { POWER_SUPPLY_PROP_STATUS, POWER_SUPPLY_PROP_HEALTH, POWER_SUPPLY_PROP_VOLTAGE_NOW, POWER_SUPPLY_PROP_CURRENT_NOW, }; static enum power_supply_property bq21061_battery_properties[] = { POWER_SUPPLY_PROP_STATUS, POWER_SUPPLY_PROP_HEALTH, }; static enum power_supply_property bq2515x_charger_properties[] = { POWER_SUPPLY_PROP_ONLINE, POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT, POWER_SUPPLY_PROP_PRECHARGE_CURRENT, POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE, POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT, POWER_SUPPLY_PROP_VOLTAGE_MAX, POWER_SUPPLY_PROP_VOLTAGE_MIN, POWER_SUPPLY_PROP_MODEL_NAME, POWER_SUPPLY_PROP_MANUFACTURER, }; static struct power_supply_desc bq2515x_mains_desc = { .name = "bq2515x-mains", .type = POWER_SUPPLY_TYPE_MAINS, .get_property = bq2515x_mains_get_property, .set_property = bq2515x_mains_set_property, .properties = bq2515x_charger_properties, .num_properties = ARRAY_SIZE(bq2515x_charger_properties), .property_is_writeable = bq2515x_power_supply_property_is_writeable, }; static struct power_supply_desc bq2515x_battery_desc = { .name = "bq2515x-battery", .type = POWER_SUPPLY_TYPE_BATTERY, .get_property = bq2515x_battery_get_property, .properties = bq2515x_battery_properties, .num_properties = ARRAY_SIZE(bq2515x_battery_properties), }; static struct power_supply_desc bq21061_battery_desc = { .name = "bq2515x-battery", .type = POWER_SUPPLY_TYPE_BATTERY, .get_property = bq2515x_battery_get_property, .properties = bq21061_battery_properties, .num_properties = ARRAY_SIZE(bq21061_battery_properties), }; static int bq2515x_power_supply_register(struct bq2515x_device *bq2515x) { struct power_supply_config psy_cfg = { .drv_data = bq2515x, }; bq2515x->mains = devm_power_supply_register(bq2515x->dev, &bq2515x_mains_desc, &psy_cfg); if (IS_ERR(bq2515x->mains)) return -EINVAL; switch (bq2515x->device_id) { case BQ25150: case BQ25155: bq2515x->battery = devm_power_supply_register(bq2515x->dev, &bq2515x_battery_desc, &psy_cfg); break; case BQ21061: bq2515x->battery = devm_power_supply_register(bq2515x->dev, &bq21061_battery_desc, &psy_cfg); break; } if (IS_ERR(bq2515x->battery)) return -EINVAL; return 0; } static int bq2515x_hw_init(struct bq2515x_device *bq2515x) { int ret = 0; if (bq2515x->init_data.ichg) ret = bq2515x_set_const_charge_current(bq2515x, bq2515x->init_data.ichg); if (ret) goto err_out; if (bq2515x->init_data.ilim) ret = bq2515x_set_ilim_lvl(bq2515x, bq2515x->init_data.ilim); if (ret) goto err_out; if (bq2515x->init_data.vreg) ret = bq2515x_set_batt_reg(bq2515x, bq2515x->init_data.vreg); if (ret) goto err_out; ret = bq2515x_disable_watchdog_timers(bq2515x); if (ret) goto err_out; err_out: return ret; } static int bq2515x_read_properties(struct bq2515x_device *bq2515x) { int ret; ret = device_property_read_u32(bq2515x->dev, "constant-charge-current-max-microamp", &bq2515x->init_data.ichg); if (ret) bq2515x->init_data.ichg = BQ2515X_DEFAULT_ICHG_UA; ret = device_property_read_u32(bq2515x->dev, "precharge-current-max-microamp", &bq2515x->init_data.iprecharge); if (ret) bq2515x->init_data.iprecharge = BQ2515X_DEFAULT_IPRECHARGE_UA; ret = device_property_read_u32(bq2515x->dev, "input-current-limit-microamp", &bq2515x->init_data.ilim); if (ret) switch (bq2515x->device_id) { case BQ25150: bq2515x->init_data.ilim = BQ25150_DEFAULT_ILIM_UA; break; case BQ25155: case BQ21061: bq2515x->init_data.ilim = BQ25155_DEFAULT_ILIM_UA; break; } ret = device_property_read_u32(bq2515x->dev, "constant-charge-voltage-max-microvolt", &bq2515x->init_data.vreg); if (ret) bq2515x->init_data.vreg = BQ2515X_DEFAULT_VBAT_REG_UV; bq2515x->ac_detect_gpio = devm_gpiod_get_optional(bq2515x->dev, "ac_detect", GPIOD_IN); if (IS_ERR(bq2515x->ac_detect_gpio)) dev_info(bq2515x->dev, "ac_detect GPIO not defined"); bq2515x->reset_gpio = devm_gpiod_get_optional(bq2515x->dev, "reset", GPIOD_OUT_LOW); if (IS_ERR(bq2515x->reset_gpio)) { if (PTR_ERR(bq2515x->reset_gpio) == -EPROBE_DEFER) return -EPROBE_DEFER; } bq2515x->lp_gpio = devm_gpiod_get_optional(bq2515x->dev, "low-power", GPIOD_OUT_LOW); if (IS_ERR(bq2515x->lp_gpio)) { if (PTR_ERR(bq2515x->lp_gpio) == -EPROBE_DEFER) return -EPROBE_DEFER; } bq2515x->ce_gpio = devm_gpiod_get_optional(bq2515x->dev, "charge-enable", GPIOD_OUT_LOW); if (IS_ERR(bq2515x->ce_gpio)) { if (PTR_ERR(bq2515x->ce_gpio) == -EPROBE_DEFER) return -EPROBE_DEFER; } return 0; } static bool bq2515x_volatile_register(struct device *dev, unsigned int reg) { switch (reg) { case BQ2515X_STAT0 ... BQ2515X_FLAG3: case BQ2515X_ADC_VBAT_M ... BQ2515X_ADC_IIN_L: return true; default: return false; } } static const struct regmap_config bq25150_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2515X_DEVICE_ID, .reg_defaults = bq25150_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25150_reg_defs), .cache_type = REGCACHE_RBTREE, .volatile_reg = bq2515x_volatile_register, }; static const struct regmap_config bq25155_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2515X_DEVICE_ID, .reg_defaults = bq25155_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25155_reg_defs), .cache_type = REGCACHE_RBTREE, .volatile_reg = bq2515x_volatile_register, }; static const struct regmap_config bq21061_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2515X_DEVICE_ID, .reg_defaults = bq21061_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq21061_reg_defs), .cache_type = REGCACHE_RBTREE, .volatile_reg = bq2515x_volatile_register, }; static int bq2515x_probe(struct i2c_client *client, const struct i2c_device_id *id) { struct device *dev = &client->dev; struct bq2515x_device *bq; int ret; bq = devm_kzalloc(dev, sizeof(*bq), GFP_KERNEL); if (!bq) return -ENOMEM; bq->client = client; bq->dev = dev; mutex_init(&bq->lock); strncpy(bq->model_name, id->name, I2C_NAME_SIZE); bq->device_id = id->driver_data; switch (bq->device_id) { case BQ25150: bq->regmap = devm_regmap_init_i2c(client, &bq25150_regmap_config); break; case BQ25155: bq->regmap = devm_regmap_init_i2c(client, &bq25155_regmap_config); break; case BQ21061: bq->regmap = devm_regmap_init_i2c(client, &bq21061_regmap_config); break; } if (IS_ERR(bq->regmap)) { dev_err(dev, "failed to allocate register map\n"); return PTR_ERR(bq->regmap); } i2c_set_clientdata(client, bq); ret = bq2515x_read_properties(bq); if (ret) { dev_err(dev, "Failed to read device tree properties %d\n", ret); goto err_out; } ret = bq2515x_hw_init(bq); if (ret) { dev_err(dev, "Cannot initialize the chip.\n"); goto err_out; } return bq2515x_power_supply_register(bq); err_out: mutex_destroy(&bq->lock); return ret; } static const struct i2c_device_id bq2515x_i2c_ids[] = { { "bq25150", BQ25150, }, { "bq25155", BQ25155, }, { "bq21061", BQ21061, }, {}, }; MODULE_DEVICE_TABLE(i2c, bq2515x_i2c_ids); static const struct of_device_id bq2515x_of_match[] = { { .compatible = "ti,bq25150", }, { .compatible = "ti,bq25155", }, { .compatible = "ti,bq21061", }, { }, }; MODULE_DEVICE_TABLE(of, bq2515x_of_match); static struct i2c_driver bq2515x_driver = { .driver = { .name = "bq2515x-charger", .of_match_table = bq2515x_of_match, }, .probe = bq2515x_probe, .id_table = bq2515x_i2c_ids, }; module_i2c_driver(bq2515x_driver); MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com>"); MODULE_AUTHOR("Ricardo Rivera-Matos <r-rivera-matos@ti.com>"); MODULE_DESCRIPTION("BQ2515X charger driver"); MODULE_LICENSE("GPL v2");