This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62840-1DLCEVM55: TPS62841

Part Number: TPS62840-1DLCEVM55

Hi,

I have downloaded the SLVMD75 and SLUM691A file from TI website. I am able to run it on OrCAD Pspice.

I am getting following issue while running in temperature Sweep mode. "ERROR(ORPSIM-16550): Floating point computation failed during matrix solution. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT INTERNAL ERROR -- Overflow, Multiply"

Do you have any idea why this issue is there in temperature Sweep mode?

Please find the attached file for more information.

I want to see the circuit behavior at -40 -20 0 25 50 and 70 degree C.

Best Regards,

Rahul